C++ code in my project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C++ code in my project

ソリューションへジャンプ
1,670件の閲覧回数
MWMinor
Contributor V

Hi

 

I'm evaluating the code warrior development environment - so a new user to this system. I have acquired a DEMO9S08AW60 board and an LCD display which I am looking to use in a new product development.

 

I would like to try writing some C++ code, but when I try to use the processor expert option in the project wizard I get a message that additional tools are required....

 

 

 

..."C++ is only available with the Professional and the standard edition when the enhanced compiler option is installed...."

 

Can any one offer assistance with this message...?

 

Where do you get these tools from and how to install them...?

 

Many thanks in advance.

 

MW

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,437件の閲覧回数
NavidadRedivivu
Contributor III

This basically means that you need the payed edition of the tools to use C++. Since you are evaluating, you might want to know that the C++ support has some known limitations. You can check this section from the compiler manual: "Known C++ Issues in the HC(S)08 Compilers".

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,438件の閲覧回数
NavidadRedivivu
Contributor III

This basically means that you need the payed edition of the tools to use C++. Since you are evaluating, you might want to know that the C++ support has some known limitations. You can check this section from the compiler manual: "Known C++ Issues in the HC(S)08 Compilers".

0 件の賞賛
返信