Bug fixes in CodeWarrior releases

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bug fixes in CodeWarrior releases

跳至解决方案
2,422 次查看
June
Contributor I

Hi,

I'm reviewing the release notes between CodeWarrior v10.4 versus v10.5. There are some known issues noted in v10.4 but not found in the bug fixes or known issues list in v10.5. May i know there's a patch for v10.4 that resolves the issues?

These are the issue IDs in question:

ENGR00250596

ENGR00184839

ENGR00243112

ENGR00252493

 

There are also some bugs listed in the compiler release note which remain to be un-resolved even in v10.7. May i know if there are plans to fix these issues?

These are the issue IDs in question:

MTWX26459

MTWX30211

 

Thanks. 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,263 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport


Hi June.


Thanks for your reply.

here is more information:

ENGR00250596 : according to CCB decision, this feature was removed.

ENGR00184839 : Improve Error Reporting. Passed validation on MCU10.5 build B130625,

ENGR00243112: Passed in MU 10.5 b130701,

ENGR00252493: SA is not supported for simulators. Added filters for all simulator configs.  solved in CW10.5  build 131201.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,263 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi June

I can confirm there are no change for these two issue, for the moment, there is no plan to change them.

MTWX26459

MTWX30211

Regarding these four:

ENGR00250596

ENGR00184839

ENGR00243112

ENGR00252493

Which version release note mentioned these issue? can you please upload the related doc. then I will check. Thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,262 次查看
June
Contributor I

Hi Jennie,

Many thanks for your reply. Regarding these issues:

ENGR00250596

ENGR00184839

ENGR00243112

ENGR00252493

They are mentioned in CodeWarrior Development Studio for Microcontrollers, v10.4 Release_Notes.pdf, Appendix A. I'm attaching the document here.

0 项奖励
回复
2,264 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport


Hi June.


Thanks for your reply.

here is more information:

ENGR00250596 : according to CCB decision, this feature was removed.

ENGR00184839 : Improve Error Reporting. Passed validation on MCU10.5 build B130625,

ENGR00243112: Passed in MU 10.5 b130701,

ENGR00252493: SA is not supported for simulators. Added filters for all simulator configs.  solved in CW10.5  build 131201.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复