Breakpoints move while editing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Breakpoints move while editing

1,417 次查看
larrycarter
Contributor I

I am using CodeWarrior and a Freedom board.  After setting a breakpoint, ANY edit of the source code above the line causes the breakpoint to stay with the editor line number and not stay with the source code line it was set on.  Thus I must delete all of my breakpoints and add new ones at the line I want to break when I go back into the debugger.  How do I get the breakpoints to stay with the source code line?

 

1) The behavior is, set a breakpoint at a line of code.  All is well.

2) Add a extra blank line in the source code above the breakpoint and recompile.

3)  When I go back into the debugger, the breakpoint jumps to line of code above its previous position.

 

Thanks for your help

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,281 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Larry:

The Eclipse environment of CodeWarrior sets the breakpoints to editor line numbers and not "code lines". So I'm afraid you are correct, you need to update your breakpoints whenever you add something above. There is no option in Eclipse to change that behavior.

Regards!

Jorge Gonzalez

0 项奖励
回复