Assembly problem  with indirect X instructions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Assembly problem  with indirect X instructions

2,254 次查看
Jim_P
Contributor III

 I am having to do a bit of Assembly coding - - for some 64 bit math - - simple add and subtract.

as I have started coding this I checked what I was doing and getting a series of error messages.

 

windows 7 64 bit CW10.1 HS08JM project

 

this is inside of a function


union DLong Add64( union DLong A, union DLong B )
    {
    static union DLong a, b, C;
    static byte D,E,F;
    byte I;
    I = 7;
    a = A;
    b = B;

    asm
        {  
       
        LDA D;
        ADD E;
        STA F;
        LDX #7
        LDA  D,x;
        ADD E, x;
        STA F, X;
        ............. more to be added
        }

    return ( C );
    }

 

error message occurs on the lines that I am trying to index using the X register.

i.e. LDA opcode16,X

 

I get the error message on the indexed opcodes of

C18123 End of Line expected

for each of the index X assembly codes

 

I have used inline assembly before without problems - - first time using indexed addressing

 

thanks Jim P

标签 (1)
标记 (1)
0 项奖励
回复
6 回复数

1,984 次查看
kef
Specialist I


Jim, I think you need to use address operator @ here:

 

        LDA  @D,x;
        ADD @E, x;
        STA @F, X;

0 项奖励
回复

1,984 次查看
Jim_P
Contributor III

Thanks that makes sense - - - - nothing else seemed to

 

I figured out a work around - - - I assigned the variables to a fixed address and then hard coded that address

worked but now what I would call ideal or right.

 

the use of the @ seems to be the key, I did try the & and that did not work.

think that part of my problem is that the variable is on the stack - - when passed. So no fixed address.

even making the variables static did not seem to help as that should have created a fixed address for the variables

 

Thanks

0 项奖励
回复

1,984 次查看
bigmac
Specialist III

Hello JP,

 

While the attached code probably does not do what you require, it does demonstrate a method of setting up a stack frame for arithmetic operations, and makes use of inline assembly code.  Maybe you will be able to extract some ideas.

 

Regards,

Mac

 

0 项奖励
回复

1,984 次查看
Jim_P
Contributor III

Thanks - I will keep the code for reference and use if the need arrives

 

Jim P

0 项奖励
回复

1,984 次查看
bigmac
Specialist III

Hello JP,

 

While it may not be the cause of your error messages, your inline code does not appear to make sense unless the variables D, E, and F are declared as arrays of at least eight elements.  You cannot assume a particular order in which the static variables are linked to memory.

 

I think that there may also be a problem with the assignments a = A; and b = B; since these are unions, and you do not specify a particular element of the union.

 

Regards,

Mac

 

0 项奖励
回复

1,984 次查看
Jim_P
Contributor III

you are looking at lots of test code trying to figure out what I am getting these errors.

 

and a union to union assignment is just fine - - - -  As A = B

note the actual code is simply a block transfer.   If assigning an int or something to a union it needs to know

what it is it is being assigned to - - - -

 

 

0 项奖励
回复