56800E CCCSClinet :Reset TO Debug : Debug Mode, Help to fix this fialed Message.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

56800E CCCSClinet :Reset TO Debug : Debug Mode, Help to fix this fialed Message.

Jump to solution
3,421 Views
samchin
Contributor I

I use USB TAP and 56800E Flash Programmer.exe for programbming MC56F8247MLH,

but no matter WIndows XP or Windows7 , this message would come out..

 

Howerver, I can't find the meaning of this message ,

and furthermore fix the prpblem ,Does anyone has similart experience and know how to fix it.

Original Attachment has been moved to: debug.log.zip

Labels (1)
0 Kudos
Reply
1 Solution
3,101 Views
TICS_Fiona
NXP Employee
NXP Employee

There is no/TRST pin on 56F8247. You can leave the /TRST open on the JTAG interface with USBTAP.

Please connect the RESET signal on the JTAG interface with GPIOD4/RESET pin on 56F8257.

You may refer to the schematic of our 56F8257 demo board:
http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/TWR-56F8257-SCH_B.pdf

Do you have a DSC demo or EVM board? To confirm this is not a software or driver problem.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,102 Views
TICS_Fiona
NXP Employee
NXP Employee

There is no/TRST pin on 56F8247. You can leave the /TRST open on the JTAG interface with USBTAP.

Please connect the RESET signal on the JTAG interface with GPIOD4/RESET pin on 56F8257.

You may refer to the schematic of our 56F8257 demo board:
http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/TWR-56F8257-SCH_B.pdf

Do you have a DSC demo or EVM board? To confirm this is not a software or driver problem.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply