56800E CCCSClinet :Reset TO Debug : Debug Mode, Help to fix this fialed Message.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

56800E CCCSClinet :Reset TO Debug : Debug Mode, Help to fix this fialed Message.

跳至解决方案
2,688 次查看
samchin
Contributor I

I use USB TAP and 56800E Flash Programmer.exe for programbming MC56F8247MLH,

but no matter WIndows XP or Windows7 , this message would come out..

 

Howerver, I can't find the meaning of this message ,

and furthermore fix the prpblem ,Does anyone has similart experience and know how to fix it.

Original Attachment has been moved to: debug.log.zip

标签 (1)
0 项奖励
回复
1 解答
2,368 次查看
TICS_Fiona
NXP Employee
NXP Employee

There is no/TRST pin on 56F8247. You can leave the /TRST open on the JTAG interface with USBTAP.

Please connect the RESET signal on the JTAG interface with GPIOD4/RESET pin on 56F8257.

You may refer to the schematic of our 56F8257 demo board:
http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/TWR-56F8257-SCH_B.pdf

Do you have a DSC demo or EVM board? To confirm this is not a software or driver problem.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,369 次查看
TICS_Fiona
NXP Employee
NXP Employee

There is no/TRST pin on 56F8247. You can leave the /TRST open on the JTAG interface with USBTAP.

Please connect the RESET signal on the JTAG interface with GPIOD4/RESET pin on 56F8257.

You may refer to the schematic of our 56F8257 demo board:
http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/TWR-56F8257-SCH_B.pdf

Do you have a DSC demo or EVM board? To confirm this is not a software or driver problem.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复