what is the single codewarrior development tool i can use for two of my products with MPC8314e  and MPU QorIQ P1013 processors respectively

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the single codewarrior development tool i can use for two of my products with MPC8314e  and MPU QorIQ P1013 processors respectively

1,185件の閲覧回数
anujkarwal
Contributor I

I need to buy a codewarrior development tool with the TAP.

Need to use for two different products having proccessors

  1. MPC8314e and
  2. MPU QorIQ P1013 respectively.

 

Please advice. Need to have it a bit urgent.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,143件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Anuj

For MPC8314e, please choose Classic CodeWarrior v8.8:

http://tinyurl.com/z9qxksw

For P1013, please choose Eclipse CodeWarrior v10.5:

http://tinyurl.com/goavdep

They are both included in the CodeWarrior Suite for NetWorked Applications:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-DS-NETAPPS

And the fact sheet is as below:
http://cache.freescale.com/files/soft_dev_tools/doc/fact_sheet/CWDEVSNETAPPFS.pdf

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信