vector redirection on HCS08 - ASM programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vector redirection on HCS08 - ASM programming

1,264件の閲覧回数
Leojunin
Contributor IV

Hello to the whole community. I'm about to use vector redirection and want to know if the compiler and linker recognizes this redirect, and correctly assigns the vectors allocated in the PRM file or should I do it myself?

ラベル(1)
0 件の賞賛
返信
1 返信

1,162件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Daniel,

There are some posts you can refer to handle this question.

Can you have a look on:

    RELOCATED INTERRUPT VECTOR TABLE

    AN4757-Migration Guide From S08 to Kinetis E Family.pdf

    ...

You can also refer to the manual provided in the tool installation.

For instance under CW for MCU V10.6.4:

    \CW MCU v10.6.4\MCU\Help\PDF\MCU_Build_Tools_Utilities.pdf -> perform a search for "Vector Table"


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信