vector address in ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vector address in ram

ソリューションへジャンプ
1,764件の閲覧回数
IlConte
Contributor IV

Dear all,

 

I have CW10-6 and S08PT60.

 

I need to redirect the serial interrupt to an address in this ram.
I tried this way but me error:

Description    Resource    Path    Location    Type

C1822 Type mismatch (expected 'void (*near )()', given 'unsigned char ')  

 


static void (* near const _vect[])(void) @0xFFB0 = { /* Interrupt vector table */

/*lint -restore Enable MISRA rule (1.1) checking. */

         UNASSIGNED_ISR,               /* Int.no. 39 Vnvm (at FFB0)                  Unassigned */

         kb1_Int,                      /* Int.no. 38 Vkbi1 (at FFB2)                 Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 37 Vkbi0 (at FFB4)                 Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 36 Vtsi (at FFB6)                  Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 35 Vrtc (at FFB8)                  Unassigned */

         isrIIC,                       /* Int.no. 34 Viic (at FFBA)                  Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 33 Vspi1 (at FFBC)                 Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 32 Vspi0 (at FFBE)                 Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 31 Vsci2tx (at FFC0)               Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 30 Vsci2rx (at FFC2)               Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 29 Vsci2err (at FFC4)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 28 Vsci1tx (at FFC6)               Used */

         UNASSIGNED_ISR,               /* Int.no. 27 Vsci1rx (at FFC8)               Used */

         UNASSIGNED_ISR,               /* Int.no. 26 Vsci1err (at FFCA)              Unassigned */

         isrVsci0tx,                   /* Int.no. 25 Vsci0tx (at FFCC)               Unassigned */

         Vector_Ram[1][0],  /*isrVsci0rx,                     Int.no. 24 Vsci0rx (at FFCE)               Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 23 Vsci0err (at FFD0)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 22 Vadc (at FFD2)                  Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 21 Vacmp (at FFD4)                 Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 20 Vmtim1 (at FFD6)                Unassigned */

         isrVmtim0,                    /* Int.no. 19 Vmtim0 (at FFD8)                Used */

         UNASSIGNED_ISR,               /* Int.no. 18 Vftm0ovf (at FFDA)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 17 Vftm0ch1 (at FFDC)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 16 Vftm0ch0 (at FFDE)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 15 Vftm1ovf (at FFE0)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 14 Vftm1ch1 (at FFE2)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 13 Vftm1ch0 (at FFE4)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 12 Vftm2ovf (at FFE6)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 11 Vftm2ch5 (at FFE8)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no. 10 Vftm2ch4 (at FFEA)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  9 Vftm2ch3 (at FFEC)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  8 Vftm2ch2 (at FFEE)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  7 Vftm2ch1 (at FFF0)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  6 Vftm2ch0 (at FFF2)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  5 Vftm2flt (at FFF4)              Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  4 Vclk (at FFF6)                  Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  3 Vlvw (at FFF8)                  Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  2 Virq_wdog (at FFFA)             Unassigned */

         UNASSIGNED_ISR,               /* Int.no.  1 Vswi (at FFFC)                  Unassigned */

         _Startup                      /* Int.no.  0 Vreset (at FFFE)                Reset vector */

};

 

How can I change the address of my address routine with ran variable ?

 

Tanks

 

Stefano

ラベル(1)
0 件の賞賛
返信
1 解決策
1,575件の閲覧回数
IlConte
Contributor IV

The solution is:

((void(*near const)(void)) &(Vector_Ram[1][0]))

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,576件の閲覧回数
IlConte
Contributor IV

The solution is:

((void(*near const)(void)) &(Vector_Ram[1][0]))

0 件の賞賛
返信