validation of DDR3 using codewarrior failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

validation of DDR3 using codewarrior failed

1,608件の閲覧回数
anshulkhare
Contributor III

Hello,

I am using T2081 and QCVS Codewarrior tool for the validation of DDR3.

While performing the test "Centring the clock" in the validation stage, I was determining the best WRLVL_START byte lane values in which 1/2 clocks of CLK_ADJ have passed for 3/4 clocks of WRLVL_START. While determining the best CLK_ADJ value in the next table as in below image it fails for all conditions including 1/2 clock .

pastedImage_1.png

Could anyone explain why are we facing the above issue.

Thanks in advance!

0 件の賞賛
返信
1 返信

1,531件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which log corresponds to the selected cell?

0 件の賞賛
返信