_timer_create_component in one more tasks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

_timer_create_component in one more tasks

Jump to solution
1,587 Views
norbertoj
Contributor III

Hi, I have the next question.

I have three tasks that need to work with timmers. So, Should I  put_timer_create_component for each task? Or, Do I need just one time in a (main) task?

 

Regardly,

 

Norberto Jiménez

Labels (1)
0 Kudos
Reply
1 Solution
1,506 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto Jiménez,

You'd better create three timer on the three tasks .

The task do not use the other tasks source .

Hope it helps

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,507 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto Jiménez,

You'd better create three timer on the three tasks .

The task do not use the other tasks source .

Hope it helps

Alice

0 Kudos
Reply