hello,everyone:
I am using the codewarrior10.7.Because I change the chip from K60FN1M0xxx12 to MK60FX512xxx12 on TWR-K60F120M by my laboratory. Do you have the kinetis 120MHZ bare metal sample which it support the chip MK60FX512xxx12 on TWR-K60F120M board?
Thanks!
Hi Minmin,
You ca download Kinetis® 120MHz bare metal sample code(REV 1.4)
from :
TWR-K60F120M|Tower System Board|Kinetis MCUs|NXP
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks,
Before,I hvae downloaded it. It just supports the chip K60FN1M0xxx12 rather than MK60FX512xxx12.
Now, I want the demo which supports MK60FX512xxx12.
Hi Minming
I don't think we have exact sample for MK60FX512xxx12. user needs refer K60FN1M0xxx12 to make MK60FX512xxx12 project.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
ok,thanks.
Hello Minmin
Hope you are working with kinetis SDK. if not then probably you will get sample examples in Kinetis SDK.
link: https://community.nxp.com/docs/DOC-329744
Let me know if any..
Thanks & regards
Harsh Patel
hello,
I am not working with kinetis SDK. I use the codewarrior10.7 for MK60FX512xxx12. Before someone give me kinetis 120MHZ bare metal sample , it support the chip K60FN1M0xxx12 on TWR-K60F120M board:Kinetis® 120MHz bare metal sample code.
Now, I just want the bare metal sample which supports the chip MK60FX512xxx12.