the demo of he chip MK60FX512xxx12 on TWR-K60F120M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the demo of he chip MK60FX512xxx12 on TWR-K60F120M

4,533 Views
minminzhengzhen
Contributor I

hello,everyone:

      I am using the codewarrior10.7.Because I change the chip from K60FN1M0xxx12 to MK60FX512xxx12 on TWR-K60F120M by my laboratory. Do you have the kinetis 120MHZ bare metal sample which it support the chip MK60FX512xxx12 on TWR-K60F120M board?

Thanks!

0 Kudos
Reply
6 Replies

1,824 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Minmin,

You ca download Kinetis® 120MHz bare metal sample code(REV 1.4)

from :

TWR-K60F120M|Tower System Board|Kinetis MCUs|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,824 Views
minminzhengzhen
Contributor I

Thanks,

Before,I hvae downloaded it. It just supports the chip K60FN1M0xxx12 rather than MK60FX512xxx12.

Now, I want the demo which supports MK60FX512xxx12.

0 Kudos
Reply

1,824 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Minming

I don't think we have exact sample for MK60FX512xxx12. user needs refer K60FN1M0xxx12 to make MK60FX512xxx12 project.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,824 Views
minminzhengzhen
Contributor I

ok,thanks.

0 Kudos
Reply

1,823 Views
harshpatel
Contributor IV

Hello Minmin

Hope you are working with kinetis SDK. if not then probably you will get sample examples in Kinetis SDK.

link: https://community.nxp.com/docs/DOC-329744 

Let me know if any..

Thanks & regards

Harsh Patel

0 Kudos
Reply

1,823 Views
minminzhengzhen
Contributor I

hello,

I am not working with kinetis SDK. I use the codewarrior10.7 for MK60FX512xxx12. Before someone give me kinetis 120MHZ bare metal sample , it support the chip K60FN1M0xxx12 on TWR-K60F120M board:Kinetis® 120MHz bare metal sample code.

Now, I just want the bare metal sample which supports the chip MK60FX512xxx12.

0 Kudos
Reply