ssoe not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ssoe not work

1,420 Views
huangqingyun
Contributor I

when i change spi(MC9S12XEP100CAG) clock edge from faling to rising edge, the spi1 module's slave select pin PH3 does not generate chip select signal(from high level to low level). but it works well when clock edge is faling edge. i was using codewarrior processor expert to develope the mcu.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,368 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Can you please specified what the falling/rising edge means in terms of POL, CPHA?

Please refer to Section 21.4.3.1 Clock Phase and Polarity Controls in the S12XE RM, rev1.25.

Anyway, the automatic slave select should work regardless of the configuration.

Could you please attach a test project?

Thank you,

BR, Daniel

0 Kudos
Reply