software emulator for S9KEAZN8AMTG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

software emulator for S9KEAZN8AMTG

ソリューションへジャンプ
1,498件の閲覧回数
navahoo
Contributor I

Which IDE have software emulator for S9KEAZN8AMTG ?  I would like to use IDE for development/debug without hardware now...

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,434件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

Unfortunately, NXP does not have a hardware emulator. However, I found the following two options you could take a look event though I don’t think there is an emulator for the specific requested device.

 

The GNU ARM Eclipse QEMU 

µTasker - Simulation examples 

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,435件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

Unfortunately, NXP does not have a hardware emulator. However, I found the following two options you could take a look event though I don’t think there is an emulator for the specific requested device.

 

The GNU ARM Eclipse QEMU 

µTasker - Simulation examples 

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信