"Debug Database Initialization" error when starting CodeWarrior 10.3 eTPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"Debug Database Initialization" error when starting CodeWarrior 10.3 eTPU

2,842 次查看
bed
Contributor II

Hello,

 

I'm getting an exception on starting CodeWarrior 10.3 eTPU (so using it to develop AND DEBUG eTPU2 code). I've reinstalled multiple times under windows 8.1 (and tried windows10 for good luck). On all starts I get an error initialising the Debug Database. CodeWarrior does continue but when I go to debug (after compiling with debug on), the Debug Tab is empty. I'm thinking it is related.

 

Has anyone else seen this error? Does anyone have a cause and a solution?

 

Thanks,

Brian

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

2,602 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Brian

There should be some problem in CodeWarrior installation. Could you please send diagnostics info? You can generate this with “File->Export->Diagnostics Information”.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 项奖励
回复