"Debug Database Initialization" error when starting CodeWarrior 10.3 eTPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Debug Database Initialization" error when starting CodeWarrior 10.3 eTPU

2,809 Views
bed
Contributor II

Hello,

 

I'm getting an exception on starting CodeWarrior 10.3 eTPU (so using it to develop AND DEBUG eTPU2 code). I've reinstalled multiple times under windows 8.1 (and tried windows10 for good luck). On all starts I get an error initialising the Debug Database. CodeWarrior does continue but when I go to debug (after compiling with debug on), the Debug Tab is empty. I'm thinking it is related.

 

Has anyone else seen this error? Does anyone have a cause and a solution?

 

Thanks,

Brian

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

2,569 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Brian

There should be some problem in CodeWarrior installation. Could you please send diagnostics info? You can generate this with “File->Export->Diagnostics Information”.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 Kudos
Reply