programme not executed after reset in code warrior 10.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

programme not executed after reset in code warrior 10.2

1,350 次查看
karanpatel
Contributor I

i am using code worrier 10.2. i develop one barebord application for pxn2020.i can able to run my application in debug mode and its working fine.but when i stop debugging and reset controller program is not there in flash.

i select debug as flash in configuration

why this is happen????

 

here i attach project....

Original Attachment has been moved to: UARTzip.zip

标签 (1)
0 项奖励
回复
1 回复

1,219 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

I need to re-install the MCU V10.2.

I don't have the pxn2020 board but a TWR-PXS2010.

I will continue to provide you feedback via the SR 1-3583394090

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复