problem with ltib on centos 6.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with ltib on centos 6.5

Jump to solution
2,802 Views
ssssss
Contributor II

hi

i have centos 6.5(final) on virtual machine and i want to run ltib on it. after running ./install script,when i run ./ltib script, there is following error :

 

 

ltib cannot be run because one or more of the host packages needed

to run it are either missing or out of date.

 

 

Please install/upgrade these packages and then re-try.

 

Package                Minimum ver   Installed info

-------                -----------   ---------------

glibc-devel            0             not installed

rpm-build              0             not installed

Died at ./ltib line 1265.

traceback:

main::host_checks:1265

  main:479

 

Started: Tue Jul 28 16:54:39 2015

Ended:   Tue Jul 28 16:54:40 2015

Elapsed: 1 seconds

 

Build Failed

 

but it seems that i have the packages.when i run yhe following command : sudo yum  install glibc-devel ,there is :

 

Loaded plugins: fastestmirror, refresh-packagekit, security

Setting up Install Process

Loading mirror speeds from cached hostfile

* base: mirror.vit.com.tr

* extras: mirror.vit.com.tr

* rpmforge: mirror.smartmedia.net.id

* updates: mirror.vit.com.tr

Package glibc-devel-2.12-1.149.el6_6.9.x86_64 already installed and latest version

Nothing to do

 

what is the problem?!

plz help me

thenks

 

mohammad

Labels (1)
0 Kudos
Reply
1 Solution
2,670 Views
ssssss
Contributor II

i switched to fedora fc 6 and it is easily done !!

thanks for your help , Pascal .

View solution in original post

0 Kudos
Reply
4 Replies
2,671 Views
ssssss
Contributor II

i switched to fedora fc 6 and it is easily done !!

thanks for your help , Pascal .

0 Kudos
Reply
2,670 Views
trytohelp
NXP Employee
NXP Employee

Hi,

To investigate the problem, we need to know exactly the CodeWarrior version you're using.

To do that you must:

  Under CodeWarrior IDE (classic)

                Start the IDE and click on Help | About Freescale CodeWarrior.

                Click on Installed Products 

                Provide us all info displayed.

                Or you can save them in a txt file.

  Under Eclipse IDE

    1-        Start Eclipse and click on Help ¦ Freescale Licenses

                The Status column gives the status of the license.

                Under Product, select it and click on details.

                A new dialog show up giving license details.

                Provide us all info displayed

    2-        Start Eclipse and click on Help ¦ About CodeWarrior Development Studio

                Under Installed Products, you will see the version used.

If the Installed Products is not available for older version you should find information in the welcome.txt

under the installation folder.

In case of MQX, please provide us the MQX version used ?

In case of BSP, please provide us the BSP info, the target and the chip used ?

In case of Ltib or PCS please provide us details about that ?

Another important information is the processor you're using.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,670 Views
ssssss
Contributor II

hi

i have codewarrior on windows but i don't have it on linux.

you mean i have to install codewarrior on linux ?

is it necessary for running ltib?! ( because i think the codewarrior on windows has no impact on installing ltib )

0 Kudos
Reply
2,670 Views
trytohelp
NXP Employee
NXP Employee

Hi,

We just need to know exactly the tools you're using.

Pascal

0 Kudos
Reply