please check your JTAG clock Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

please check your JTAG clock Speed

3,534 Views
刘乐乐
Contributor I

安装了codewarrior以及补丁后  连接仿真器至8308   Tools -> Flash programmer 中也配置了相应参数 到达Erase /Blank check 点击Erase 后  出现:please check your JTAG clock Speed .      仿真器的TX/RX灯始终是绿色闪烁    RUN/PAUSE始终是红色常亮

安装版本:CW_Power_Architecture_V8.8_Build_80229

补丁版本:CW_PA_8_8_3_Build_90619

仿真器编号 TDA5879

0 Kudos
Reply
1 Reply

2,981 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 刘 乐乐 ,

First please download and install Patch 8.8.6 to update CCS USB driver to support CodeWarrior TAP USB connection.

Please login www.nxp.com, click MY ACCOUNT->Software Licensing and Support->CodeWarrior*Suite*->

8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

If there is no valid RCW on the target board, please use CodeWarrior JTAG configuration file. Please configure CW JTAG configuration file from Edit->Debug Version Settings->Debugger->Remote Debugging->Edit Connection->Use JTAG Configuration file, JTAG configuration files are located in C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Support\Initialization_Files\jtag_chains.

For flash programming, please refer to the attached ppt.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply