main.c code disappears when building for the first time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

main.c code disappears when building for the first time

1,905件の閲覧回数
juanignaciotroi
Contributor III

Hello

 

Each time I open the CW v10.6, the first time I build my project, the code written in the main.c file, and inside the infinite loop [ for(;;){ MY CODE } ] disappears and the following window appears:

 

Why does this happen? Is it possible to avoid this things happening?

 

Thank you very much

 

Juan Ignacio Troisi

ラベル(1)
0 件の賞賛
返信
1 返信

1,839件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi, Juan,

I see you're using Processor Expert.

What is the tool version you're using ?

According to the info provided in the status bar, some updates can be apply.

To avoid problem we recommend to apply them.

If you want keep a copy of this current installation, you can copy the installation folder before to install updates.

If the update will not solve the problem, can you please provide me the main.c file ?


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信