interface between K20D50M with a sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interface between K20D50M with a sensor

1,909件の閲覧回数
sosopavliashvil
Contributor I

Hi all,

 

I am really new to microcontrollers. I am trying to interface K20D50M with a capacitance sensor. I was wandering if there are any demo projects that I can use.

Here is the serial data format of the capacitance sensor:

 

The ASCII output from TXD pin of J4 contains three fields: sequence number, measurement time (in seconds), and measured capacitance. The line format is as below.

SSSSS TTTTT.tt CCCCU

where ‘SSSSS’is 5 digit sequence number, ‘TTTTT.tt’is 8 digit time stamp (in second), and CCCCU is 5 digit measured capacitance with U being unit digit. Different fields are separated by 1 space. Each line is ended with ‘LF’(0x0A) and ‘CR’(0x0D). Output baud rate is 38400bps fixed. Data format is 8 data bits, 1 stop bit, and no parity.

Output level is 5V. So a level converter is needed to connect to RS232 compatible device (PC serial port, for example).


Could you please send me If you have any demo projects that would be helpful

Thank you and have a great day

ラベル(1)
0 件の賞賛
返信
1 返信

1,857件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Please give a check to the answer provided in the next thread:

Kinetis K20D50M interface with Capacitance sensor

Regards!

Jorge Gonzalez

0 件の賞賛
返信