how to output the build result to the log.txt through file redirection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to output the build result to the log.txt through file redirection

2,007 Views
kevinding
Contributor I

Using the Dos command "CmdIDE_PATH="C:\Program Files (x86)\Freescale\CWS12v5.1\bin\CmdIDE.exe" /r /b /c Project.mcp > log.txt" to automatically building the created project. but I cannot output put the such as "No error,<Code 0>" to the log.txt, How can I get it, thank you.

0 Kudos
Reply
1 Reply

1,862 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kevin

Attached video is for how to use file redirection command. FYI.

I use the demo code under CW5.1 install folder.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply