how to debug WCT 5WTXAUTO with CodWarrior TAP Probe(CWH-CTP-STC-YE-SCH)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to debug WCT 5WTXAUTO with CodWarrior TAP Probe(CWH-CTP-STC-YE-SCH)

ソリューションへジャンプ
2,601件の閲覧回数
santoshpulasani
Contributor III

Hi Team NXP,

 

Working with WCT 5WTXAUTO board for wireless charging. Can you please sujjest which connecting probe to use i have already ordered CWH-CTP-STC-YE-SCH and CWH-CTP-COP-YE-SCH.

 

For debugging I am using Codewarrior TAP.

 

 

Since I habe J4 (14 pin) JTAG on my WCT 5WTXAUTO board i have ordered 14 pin CWH-CTP-STC-YE-SCH but  the 8th pin is completely covered .i.e unable to plug into the J4 cpnnector of WCT 5WTXAUTO board.

 

 

Best Regards,

Santosh Reddy Pulasani

ラベル(1)
1 解決策
2,251件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Santosh

Pin7 and Pin8 can be disconnected on JTAG interface. So please remove or cut off the pin 8 of J4 WCT on 5WTXAUTO board.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,252件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Santosh

Pin7 and Pin8 can be disconnected on JTAG interface. So please remove or cut off the pin 8 of J4 WCT on 5WTXAUTO board.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,251件の閲覧回数
santoshpulasani
Contributor III

Hello Fiona,

A Big Thank you for the sujjestion .It was helpfull .

Now able to flash programs into microprocessor of 5WTXAUTO board.

Best Regards,

Santosh Reddy Pulasani

0 件の賞賛
返信