help !!!I can't unsecure the 9S12GN32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help !!!I can't unsecure the 9S12GN32

1,152 Views
seawind_hit_77
Contributor I

hello everyone! I have a problem, in codewarrior, i want to unsecure the s9S12GN32  0N48A and erase all blcok, but the flash is unchanged, and the content is the same as the original, what is the problem?

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

the flash is unchanged!!!!

Labels (1)
0 Kudos
Reply
1 Reply

1,079 Views
RadekS
NXP Employee
NXP Employee

Hi Liu,

I am not sure whether it is a reason for your issue, but the default P&E_Multilink_USB_Erase_unsecure_hcs12p.cmd file contains reset command prior unsecure.
After reset, the bus clock (source for flash clock) is 6.25MHz. Therefore, you should set FCLKDIV to 5, instead of 16.

Please try correct FCLKDIV value.

If that will not work, please try Unsecure12 tool directly from PEmicro (when you use PEmicro or OSBDM debugger).

http://www.pemicro.com/downloads/download_file.cfm?download_id=16 

Sometimes, this could help.

I hope it helps you.

Have a great day,
Radek

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply