generate S record file with no RAM information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

generate S record file with no RAM information

1,334 Views
cabl
Contributor III

Does anybody know if it´s possible to generate the s-record file without information about the RAM memory areas? Let´s focus on DSC, if it makes a difference.

 

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

1,242 Views
TICS_Fiona
NXP Employee
NXP Employee

Whether the S-record file includes the data in RAM depends on the link command file in project.  Please modify the link command file in order to place the code and all constants and global variables into RAM.

Best Regards

Fiona

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply