gcc-4.8.2 for e6500 linux ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gcc-4.8.2 for e6500 linux ?

18,544件の閲覧回数
guydurrieu
Contributor I

Hi,

 

I currently experiment  Qorl T4240 with CodeWarrior v10.4 (both bareboard and linux). There is no gcc linux toolchain installed, so I tried to install one. However I found only a gcc-4.7.2 service pack, and CodeWarrior search only  gcc-4.8.2. Is it possible to obtain somewhere the gcc-4.8-2 service pack or to let CodeWarrior v10.4 work with gcc-4.7.2 (I tried several ways, but didn't succeed) ?

 

Thanks in advance for your help !

 

-- GD.

ラベル(1)
タグ(3)
0 件の賞賛
返信
14 返答(返信)

17,764件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Guy,

I've installed PA v10.4 last week.

I've created a default project with the project wizard.

Running the Help + Install new software I see:

pastedImage_1.png

Selecting the Project properties I see:

pastedImage_0.png


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,764件の閲覧回数
guydurrieu
Contributor I

Le 11/12/2014 16:23, Durrieu Guy a écrit :

Le 11/12/2014 15:59, Pascal Irrle a écrit :

>> Hi Guy,

>>

>>

>>

>> I've installed PA v10.4 last week.

>>

>> I've created a default project with the project wizard.

>>

>>

>>

>> Running the Help + Install new software I see:

>>

>> https://community.freescale.com/servlet/JiveServlet/downloadImage/2-461855-17525/pastedImage_1.png

>> <https://community.freescale.com/servlet/JiveServlet/showImage/2-461855-17525/pastedImage_1.png>

>>

>>

>>

>>

>>

>> Selecting the Project properties I see:

>>

>> https://community.freescale.com/servlet/JiveServlet/downloadImage/2-461855-17524/pastedImage_0.png

>> <https://community.freescale.com/servlet/JiveServlet/showImage/2-461855-17524/pastedImage_0.png>

>>

>>

>> Have a great day,

>> Pascal

>> Freescale Technical Support

Thanks !

Regards.

Finally, it seems it is again the gcc-4.7.2-XMe6500-linux version which

is within the pack...

Regards.

-- GD.

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

Guy DURRIEU e-mail [email protected]

ONERA

Département Traitement de l'Information et Modélisation

CEntRe de Toulouse, 2, avenue Edouard Belin B.P. 74025

31055 TOULOUSE CEDEX 4 FRANCE

tel (33) 05.62.25.26.59 fax (33) 05.62.25.25.93

avertissement http://www.onera.fr/onera-en/emails-terms

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

0 件の賞賛
返信

17,764件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Guy,

The tool can be checked in the installation.

On my side under \CW_PA_v10.4.0\Cross_Tools folder I see:

Open a command prompt to and check the version:

E:\Freescale\CW_PA_v10.4.0\Cross_Tools\gcc-4.8.2-Ee6500-aeabi\bin>powerpc-aeabi-

gcc.exe -v

Using built-in specs.

COLLECT_GCC=powerpc-aeabi-gcc.exe

COLLECT_LTO_WRAPPER=e:/freescale/cw_pa_v10.4.0/cross_tools/gcc-4.8.2-ee6500-aeab

i/bin/../libexec/gcc/powerpc-aeabi/4.8.2/lto-wrapper.exe

Target: powerpc-aeabi

Configured with: ../src_gcc/configure --build= --target=powerpc-aeabi --host=i68

6-mingw32 --with-long-double-128 --enable-poison-system-directories --with-gnu-a

s --with-gnu-ld --disable-libstdcxx-pch --disable-libssp --disable-libmudflap --

disable-bootstrap --disable-libquadmath --disable-nls --enable-symvers=gnu --ena

ble-__cxa_atexit --enable-threads --prefix=/opt/freescale/gcc-4.8.2-Ee6500-aeabi

/i686-mingw32 --with-sysroot=/opt/freescale/gcc-4.8.2-Ee6500-aeabi/i686-mingw32/

powerpc-aeabi --with-build-sysroot=/tmp/b30502/release//opt/freescale/gcc-4.8.2-

Ee6500-aeabi/i686-mingw32/powerpc-aeabi --with-build-time-tools=/tmp/b30502/rele

ase//opt/freescale/gcc-4.8.2-Ee6500-aeabi/i686-mingw32/powerpc-aeabi/bin --enabl

e-languages=c,c++,fortran --disable-shared --disable-threads --with-newlib --wit

h-headers=yes --with-cpu-32=e6500 --with-cpu-64=e6500 --enable-powerpc-e500mc-ae

abi --enable-targets=all --enable-languages=c,c++ --with-host-libstdcxx='-static

-libgcc -Wl,-Bstatic,-lstdc++,-Bdynamic -L/tmp/b30502/release//opt/freescale/ELe

6500/mingw32_host_libs/usr/lib -lintl -lm' --with-gmp=/tmp/b30502/release//opt/f

reescale/ELe6500/mingw32_host_libs/usr --with-mpfr=/tmp/b30502/release//opt/free

scale/ELe6500/mingw32_host_libs/usr --with-mpc=/tmp/b30502/release//opt/freescal

e/ELe6500/mingw32_host_libs/usr --with-ppl=/tmp/b30502/release//opt/freescale/EL

e6500/mingw32_host_libs/usr --with-isl=/tmp/b30502/release//opt/freescale/ELe650

0/mingw32_host_libs/usr --with-cloog=/tmp/b30502/release//opt/freescale/ELe6500/

mingw32_host_libs/usr --enable-cloog-backend=isl --with-libiconv-prefix=/tmp/b30

502/release//opt/freescale/ELe6500/mingw32_host_libs/usr

Thread model: single

gcc version 4.8.2 20131016 (Thu Mar 13 11:42:43 CDT 2014        build.sh rev=96

3 s=F482 ELe6500 -V release_r963_build_Fed_ELe6500) (GCC)

E:\Freescale\CW_PA_v10.4.0\Cross_Tools\gcc-4.8.2-Ee6500-aeabi\bin>


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,764件の閲覧回数
guydurrieu
Contributor I

Le 12.12.2014 14:36, Pascal Irrle a écrit :

GCC-4.8.2 FOR E6500 LINUX ?

reply from Pascal Irrle in CodeWarrior Development Tools - View

the full discussion

0 件の賞賛
返信

17,764件の閲覧回数
trytohelp
NXP Employee
NXP Employee

I've installed the following patches:

pastedImage_2.png

After that, I've created a project with the wizard:

        File + New + CodeWarrior Linux Project wizard

        Select QorIQ_T4 + T4240

now the tool chain Linux: GCC LINUX e6500 is available.

pastedImage_3.png


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,749件の閲覧回数
guydurrieu
Contributor I

Le 15/12/2014 14:48, Pascal Irrle a écrit :

After that, I've created a project with the wizard:

File + New + CodeWarrior Linux Project wizard

Select QorIQ_T4 + T4240

now the tool chain Linux: GCC LINUX e6500 is available.

Hi Pascal,

Thanks for your help.

I can see the packages you indicate, but when I try to install them, I

get errors (see joint screenshot).

In the details window:

-


Software being installed: Service Pack for Windows GCC Linux-GNU Build

Tool version 4.4-209 4.8.2

(com.freescale.GccLinuxgnu.4.4-209.win.sp.feature.group 4.8.2)

Missing requirement: Service Pack for Windows GCC Linux-GNU Build Tool

version 4.4-209 4.8.2

(com.freescale.GccLinuxgnu.4.4-209.win.sp.feature.group 4.8.2) requires

'com.freescale.pa.gcc.linuxgnu.toolchain 10.0.0' but it could not be found

-


Regards.

-- GD.

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

Guy DURRIEU e-mail [email protected]

ONERA

Département Traitement de l'Information et Modélisation

CEntRe de Toulouse, 2, avenue Edouard Belin B.P. 74025

31055 TOULOUSE CEDEX 4 FRANCE

tel (33) 05.62.25.26.59 fax (33) 05.62.25.25.93

avertissement http://www.onera.fr/onera-en/emails-terms

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

0 件の賞賛
返信

17,749件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Guy,

I've re-installed the GCC linux tool chain on a clean PA V10.4.

To be installed I've executed 2 times the process.

To be done the installation requires more than 2 hours on my side.

Attached a video showing the process.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,749件の閲覧回数
guydurrieu
Contributor I

Le 19/12/2014 08:01, Pascal Irrle a écrit :

Hi Guy,

I've re-installed the GCC linux tool chain on a clean PA V10.4.

To be installed I've executed 2 times the process.

To be done the installation requires more than 2 hours on my side.

Attached a video showing the process.

Hi Pascal,

Thanks for your help.

I had a look to your video and retried the install, but still remain

stuck to the same problem (see screeshot). I don't even reach the

license step.

Same diagnosis in the "Details window":

-


Cannot complete the install because one or more required items could not

be found.

Software being installed: Service Pack for Linux GCC Linux-GNU Build

Tool version 4.4-209 4.7.2

(com.freescale.GccLinuxgnu.4.4-209.lin.sp.feature.group 4.7.2)

Missing requirement: Service Pack for Linux GCC Linux-GNU Build Tool

version 4.4-209 4.7.2

(com.freescale.GccLinuxgnu.4.4-209.lin.sp.feature.group 4.7.2) requires

'com.freescale.pa.gcc.linuxgnu.toolchain 10.0.0' but it could not be found

-


Regards.

-- GD.

P.S: I selected the "lin" repositories, but the result is identical with

the "win" ones.

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

Guy DURRIEU e-mail [email protected]

ONERA

Département Traitement de l'Information et Modélisation

CEntRe de Toulouse, 2, avenue Edouard Belin B.P. 74025

31055 TOULOUSE CEDEX 4 FRANCE

tel (33) 05.62.25.26.59 fax (33) 05.62.25.25.93

avertissement http://www.onera.fr/onera-en/emails-terms

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

0 件の賞賛
返信

17,749件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Guy,

Strange.

Can you try it with a new PA v10.4 installation ?

I've performed it under Win 7 64 bit OS + CW for PA v10.4 (Windows).


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,749件の閲覧回数
guydurrieu
Contributor I

Le 19/12/2014 10:26, Pascal Irrle a écrit :

Guy,

Strange.

Can you try it with a new PA v10.4 installation ?

I've performed it under Win 7 64 bit OS + CW for PA v10.4 (Windows).

Strange indeed.

I reinstalled PA v10.4. Same problem again. Then I switched to a new

empty workspace, and things seem to go better. Cannot understand why.

Anyway, Thanks for your help !

Regards.

-- GD.

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

Guy DURRIEU e-mail [email protected]

ONERA

Département Traitement de l'Information et Modélisation

CEntRe de Toulouse, 2, avenue Edouard Belin B.P. 74025

31055 TOULOUSE CEDEX 4 FRANCE

tel (33) 05.62.25.26.59 fax (33) 05.62.25.25.93

avertissement http://www.onera.fr/onera-en/emails-terms

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

0 件の賞賛
返信

17,749件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Guy,

On my side I met similar problem.

I performed the process several times.

I will re-install a clean PA V10.4 instance and will provide you more info to install all needed patches.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

17,749件の閲覧回数
trytohelp
NXP Employee
NXP Employee

It seems we can install it:

pastedImage_0.png

I've launched the installer ...

0 件の賞賛
返信

17,749件の閲覧回数
guydurrieu
Contributor I

Le 11/12/2014 15:59, Pascal Irrle a écrit :

Hi Guy,

I've installed PA v10.4 last week.

I've created a default project with the project wizard.

Running the Help + Install new software I see:

https://community.freescale.com/servlet/JiveServlet/downloadImage/2-461855-17525/pastedImage_1.png

<https://community.freescale.com/servlet/JiveServlet/showImage/2-461855-17525/pastedImage_1.png>

Selecting the Project properties I see:

https://community.freescale.com/servlet/JiveServlet/downloadImage/2-461855-17524/pastedImage_0.png

<https://community.freescale.com/servlet/JiveServlet/showImage/2-461855-17524/pastedImage_0.png>

Have a great day,

Pascal

Freescale Technical Support

Thanks !

Regards.

-- GD.

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

Guy DURRIEU e-mail [email protected]

ONERA

Département Traitement de l'Information et Modélisation

CEntRe de Toulouse, 2, avenue Edouard Belin B.P. 74025

31055 TOULOUSE CEDEX 4 FRANCE

tel (33) 05.62.25.26.59 fax (33) 05.62.25.25.93

avertissement http://www.onera.fr/onera-en/emails-terms

=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=

0 件の賞賛
返信

17,749件の閲覧回数
addiyi
NXP Employee
NXP Employee

Try to use this update site: http://freescale.com/lgfiles/updates/Eclipse/PA10_4_0/com.freescale.pa.buildtools_win. It is already available in Install New Software and will provide option for PA GCC 4.8.2-r963 toolchain to be installed.

Adrian

0 件の賞賛
返信