fail to program to s29gl256p flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fail to program to s29gl256p flash

3,263 Views
konduripraveen
Contributor II

hi all,

          iam currently working on powerpc mpc8321E board and iam facing problem at programming into the s29gl256p flash through codewarrior 8.8. the log file of code warrior shows like this

 

 

 

: -------------------------

 

Using restricted address range 0xFE000000 to 0xFFFFFFFF

 

Programming file C:\Documents and Settings\nomus\Desktop\new\u-boot.bin

Trying auto-detect...

  File is NOT of type Motorola S-Record Format.

  File is NOT of type Elf Format.

Auto-detection is successful.

  File is of type Binary/Raw Format.

 

Using Algorithm: amd16x1.elf

 

 

 

======================================================================

=== Target Configuration Settings

=== Connection:       CodeWarrior USB TAP

=== Target Processor: 8321

=== Target Init File: E:\u_boot\UBOOT\832xMDS_init.cfg

======================================================================

Connecting......Connected

 

 

======================================================================

=== Execute: Program

=== Timestamp:  Wed Sep 23 15:19:11 2015

=== Flash Device:         S29GL256P

=== Flash Organization:   16Mx16x1

=== Flash Mem Start Addr: 0xFE000000

=== Flash Mem End Addr:   0xFFFFFFFF

======================================================================

Informing other connection clients that the target is being 'clobbered'.

Loading Flash Device Driver at: 0x00002000

Flash Driver Buffer is at:      0x00003D70

Flash Driver Buffer Size is:    0x0000E290

Done

 

Initialization Command Succeeded

Trying auto-detect...

  File is NOT of type Motorola S-Record Format.

  File is NOT of type Elf Format.

Auto-detection is successful.

  File is of type Binary/Raw Format.

 

Programming 0x00010000 bytes of Target Memory at 0xFFF00000

 

after this nothing will happend i am unable to find the reason of this, could anybody help me in finding the reason behind this ?

 

thanks & regards

praveen

Labels (1)
0 Kudos
Reply
4 Replies

2,892 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello konduri praveen,

I didn't fine erase action in your flash programming log, is the above a whole log, the first step of flash programming algorithm should be reading the flash ID, this is not included in the above log either.

The initialization file provided in CodeWarrior 8.8 is only used for Freescale demo board, you need to customize the .cfg file according to your target board.

Would you please also provide 832xMDS_init.cfg which you used?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,892 Views
konduripraveen
Contributor II

hello Yiping Wang

              please give reply to question.

Thankyou

K.Praveen

0 Kudos
Reply

2,892 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello konduri praveen,

I didn't find obvious problem in your initialization file, but I found another problem, you use the algorithm amd16x1.elf to do flash programming, please refer to the following section of s29gl256p device definition from CodeWarrior 8.8, the algorithm S29GL-P_16x1.elf is used rather than amd16x1.elf. Actually the device s29gl256p has already been included in CodeWarrior 8.8, no need to define its configuration in CodeWarrior 8.8 by yourself.

  <organizationcount>6</organizationcount>

  <organization>32Mx8x1</organization>

  <organization>32Mx8x2</organization>

  <organization>32Mx8x4</organization>

  <organization>16Mx16x1</organization>

  <organization>16Mx16x2</organization>

  <organization>16Mx16x4</organization>

  <id>22</id>

  <id>22</id>

  <id>22</id>

  <id>227E</id>

  <id>227E</id>

  <id>227E</id>

  <algorithm>amd8x1alt.elf</algorithm>

  <algorithm>amd8x2alt.elf</algorithm>

  <algorithm>amd8x4alt.elf</algorithm>

  <algorithm>S29GL-P_16x1.elf</algorithm>

  <algorithm>amd16x2.elf</algorithm>

  <algorithm>amd16x4.elf</algorithm>


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,891 Views
konduripraveen
Contributor II

hello Yiping Wang,

    thanks for your reply , while programming into the flash i am not erasing it through the freescale codewarrior tool for that i am using the console code of bootloader,  these are some of the observations that i observed in codewarrior,

1. while reading from hardware diagnostics  i am able to read that all the content is been cleared (FFFF).

2. erase the complete flash is sucessful but while doing the blank check its getting struck at some sector which is not fixed.

3. erasing the particular sector and blank check is sucessful.

4. its getting struck after

Programming 0x00010000 bytes of Target Memory at 0xFFF00000

    while programming through codewarrior

please find the attached 832xMDS_init.cfg file.

thanks again for your reply

Thanks & Regards

Konduri Praveen

0 Kudos
Reply