erase method FlexNVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

erase method FlexNVM

1,274 Views
pierluigirosset
Contributor I

Hi team,

I 'd like to know some feature on the MK20DX256VLL10 about Flexmemory.

The device has 512KB total Flash, where 256KB are Flash and 256KB are FlexNVM,  and 64KB SRAM plus 4KB  EEPROM/FlexRam.

 

My question is:  I use part or full FlexNVM as Flash  and now  Can I to Erase single sector or I must entire block?

Which is  the minimun erasable memory space in FlexNVM as normal flash for  this device?

 

Ciao

Piggi

Labels (1)
0 Kudos
Reply
1 Reply

1,171 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

In the reference manual of MK20DX256VLL10 chip , there is little about erase the flashNVM.

While i think you can refer to this manual "K20P64M72SF1RM.pdf" , this is about the MK20DX256VLH7, they are only the frequency is different.

On this RM, we can see :

pastedImage_0.png

this meaning in the flexNVM, the minimum erase size is 1 Kbyte.

Hope it helps

Alice

0 Kudos
Reply