erase method FlexNVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

erase method FlexNVM

1,297 次查看
pierluigirosset
Contributor I

Hi team,

I 'd like to know some feature on the MK20DX256VLL10 about Flexmemory.

The device has 512KB total Flash, where 256KB are Flash and 256KB are FlexNVM,  and 64KB SRAM plus 4KB  EEPROM/FlexRam.

 

My question is:  I use part or full FlexNVM as Flash  and now  Can I to Erase single sector or I must entire block?

Which is  the minimun erasable memory space in FlexNVM as normal flash for  this device?

 

Ciao

Piggi

标签 (1)
0 项奖励
回复
1 回复

1,194 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

In the reference manual of MK20DX256VLL10 chip , there is little about erase the flashNVM.

While i think you can refer to this manual "K20P64M72SF1RM.pdf" , this is about the MK20DX256VLH7, they are only the frequency is different.

On this RM, we can see :

pastedImage_0.png

this meaning in the flexNVM, the minimum erase size is 1 Kbyte.

Hope it helps

Alice

0 项奖励
回复