dongle license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dongle license

2,215件の閲覧回数
randybulloch
Contributor III

Hi All,

I have a CW "BASIC" dongle license which stopped working.  I am using CW10.5, Win7, 64bit. I have an active service request, 1-1251046487,

lots of response but no fix. My favorite FS employee is taking a short vacation and I prefer the open forum anyway.  I have tried re-installing, etc. with no luck for almost 2 weeks.

The LmTools Utility shows the correct "FLEXID" but builds fail with a message that the code exceeds the size of the license. The code is less than

the 512k available for the Kenitis K BASIC license so it should build.

 

Is it correct that if the correct FLEXID for the dongle appears in the LMTOOL that the license should work?

 

How do I know that I have a "good" license file?

 

Any suggestions? 

 

Randy

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,022件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Randy,

Most of the time when the USBdongle ID is displayed in the FlexID field under Lmtools, the USBdongle should be correctly installed. However in some case I've already met problem on customer side ...

Under Eclipse the best way to see if a license file is correctly used is to:

      - launch Eclipse,

      - click on Help + Freescale License,

      - select license and click on details.

a dialog containing license info will be displayed.

Regards

Pascal

0 件の賞賛
返信

2,022件の閲覧回数
randybulloch
Contributor III

Hi Pascal,

Yes, I agree this is what I see now that the license works. When it was

NOT working, there was no "Freescale License" selection under Help.

In a message dated 1/8/2014 8:07:02 A.M. Central Standard Time,

[email protected] writes:

(https://community.freescale.com/)

dongle license

reply from Pascal Irrle

(https://community.freescale.com/people/trytohelp?et=watches.email.thread) in CodeWarrior Development Tools - _View the

full discussion_

(https://community.freescale.com/message/372056?et=watches.email.thread#372056)

0 件の賞賛
返信