does anybody have a dsp56805 config file for flash programmer v1.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does anybody have a dsp56805 config file for flash programmer v1.2?

ソリューションへジャンプ
1,972件の閲覧回数
danielmak
Contributor I

Does anybody have a DSP56805 config file for Flash Programmer v1.2?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,700件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

56800E Flash Programmer only works for 56800E, and it doesn't not support 56800 product.

To program DSP56F805, please use CodeWarrior, or flash_over_jtag.

CodeWarrior v8.3 can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

It supports programming with USBTAP and Parallel.

flash_over_jtag is a command-line tool, however it does not support USBTAP. And it does not work on Windows 7.

I attached this tool.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,700件の閲覧回数
ruvimelaver
Contributor II

Hello Fiona,

Thanks for your reply .

I tried to work with the "DCS Flasher" using the GUI ,but I am getting an error which I am not getting using CodeWarrior  .

================================

Using the "DCS Flasher"  I Do a Program/Verify I get the following message :

================================

Performing PROGRAM operation on MC56F84789 through the UTAP . . .

Error 1: Unaligned srecord at C:/work/Bootloader/uC/Bootloader/MC56F84789_Internal_PFlash_LDM/56F84789_Bootloader.elf.S:271: "S30B0001F3FDCDAB3412FF0046" .

=============================================

But when I am using the Flash operation using the Codewarrior  I do not get any Error , please see the following :

154538_154538.pngpastedImage_1.png

Console output :

====================================

fl::target -lc "LC for Simple Flash"

fl::target -b 0x60400 0x1000

fl::target -v off -l off

cmdwin::fl::device -d "MC56F84789_P_FLASH" -o "144kx16x1" -a 0x0 0x6bfff

cmdwin::fl::image -f "C:\\work\\Bootloader\\uC\\Bootloader\\MC56F84789_Internal_PFlash_LDM\\56F84789_Bootloader.elf.S" -t "Auto Detect" -re on -r 0x0 0x6bfff -oe off

cmdwin::fl::erase image

Beginning Operation ... 

-------------------------

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Performing target initialization ... 

Erasing ......

Erase Command Succeeded.

cmdwin::fl::write

Beginning Operation ... 

-------------------------

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Programming ...

Program Command Succeeded 

Flash Operation. done

cmdwin::fl::device -d "MC56F84789_X_FLASH" -o "152kx16x1" -a 0x8000 0x3ffff

cmdwin::fl::image -f "C:\\work\\Bootloader\\uC\\Bootloader\\MC56F84789_Internal_PFlash_LDM\\56F84789_Bootloader.elf.S" -t "Auto Detect" -re on -r 0x8000 0x3ffff -oe off

cmdwin::fl::erase image

Beginning Operation ... 

-------------------------

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Nothing to erase.  No sectors selected

Erase Command Succeeded.

cmdwin::fl::write

Beginning Operation ... 

-------------------------

Flash Operation.  ...

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Programming ...

Programming warning.  No data to be programmed in selected flash memory range.

Program Command Succeeded 

Flash Operation. done

fl::target -lc "LC for Simple Flash"

fl::target -b 0x60400 0x1000

fl::target -v off -l off

cmdwin::fl::device -d "MC56F84789_P_FLASH" -o "144kx16x1" -a 0x0 0x6bfff

cmdwin::fl::erase all

Beginning Operation ... 

-------------------------

Performing target initialization ... 

Erasing ..........

Erase Command Succeeded.

cmdwin::fl::device -d "MC56F84789_X_FLASH" -o "152kx16x1" -a 0x8000 0x3ffff

cmdwin::fl::erase all

-------------------------

Erasing ..........

Erase Command Succeeded.

cmdwin::fl::device -d "MC56F84789_P_FLASH" -o "144kx16x1" -a 0x0 0x6bfff

cmdwin::fl::blankcheck all

Beginning Operation ... 

-------------------------

Flash Operation.

Blank Checking ..........

BlankCheck Command Succeeded.

cmdwin::fl::device -d "MC56F84789_X_FLASH" -o "152kx16x1" -a 0x8000 0x3ffff

cmdwin::fl::blankcheck all

Beginning Operation ... 

-------------------------

Flash Operation.

Blank Checking ..........

BlankCheck Command Succeeded.

fl::target -lc "LC for Simple Flash"

fl::target -b 0x60400 0x1000

fl::target -v off -l off

cmdwin::fl::device -d "MC56F84789_P_FLASH" -o "144kx16x1" -a 0x0 0x6bfff

cmdwin::fl::image -f "C:\\work\\Bootloader\\uC\\Bootloader\\MC56F84789_Internal_PFlash_LDM\\56F84789_Bootloader.elf.S" -t "Auto Detect" -re on -r 0x0 0x6bfff -oe off

cmdwin::fl::erase image

Beginning Operation ... 

-------------------------

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Performing target initialization ... 

Erasing ......

Erase Command Succeeded.

cmdwin::fl::write

Beginning Operation ... 

-------------------------

Flash Operation.  ...

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Programming ...

Program Command Succeeded 

Flash Operation. done

cmdwin::fl::device -d "MC56F84789_X_FLASH" -o "152kx16x1" -a 0x8000 0x3ffff

cmdwin::fl::image -f "C:\\work\\Bootloader\\uC\\Bootloader\\MC56F84789_Internal_PFlash_LDM\\56F84789_Bootloader.elf.S" -t "Auto Detect" -re on -r 0x8000 0x3ffff -oe off

cmdwin::fl::erase image

Beginning Operation ... 

-------------------------

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Nothing to erase.  No sectors selected

Erase Command Succeeded.

cmdwin::fl::write

Beginning Operation ... 

-------------------------

Flash Operation.  ...

Auto-detection is successful.

  File is of type Motorola S-Record Format.

Programming ...

Programming warning.  No data to be programmed in selected flash memory range.

Program Command Succeeded 

Flash Operation. done

================================

Please advise if you have a solution as I need to give our production line an easy tool for programming ( via command line ...batch ...)

Thanks again

Ruvi

0 件の賞賛
返信
1,700件の閲覧回数
ruvimelaver
Contributor II

Hello ,

Please advise if I can program the MC56F84789 using this tool as I did not see the .cfg file for the item.

Thanks

Ruvi

0 件の賞賛
返信
1,700件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Ruvi

56800E Flash Programmer does not support MC56F84789.

To program MC56F84789, user can use CodeWarrior for MCU10.6.4's built in flash programmer. CodeWarrior v10.6.4 can be downloaded from

http://tinyurl.com/6jo5tge

Or choose P&E's Cyclone MAX:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=145

Or you can use DSC Flasher to program 56F84789. Please search 'AN4824' on NXP website (www.nxp.com) to download this tool and help document.  It is a free tool.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 件の賞賛
返信
1,701件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

56800E Flash Programmer only works for 56800E, and it doesn't not support 56800 product.

To program DSP56F805, please use CodeWarrior, or flash_over_jtag.

CodeWarrior v8.3 can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

It supports programming with USBTAP and Parallel.

flash_over_jtag is a command-line tool, however it does not support USBTAP. And it does not work on Windows 7.

I attached this tool.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信