dmitry konkov

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dmitry konkov

4,123 Views
kdo
Contributor I

How to install processor expert 

0 Kudos
Reply
4 Replies

4,006 Views
Pavel
NXP Employee
NXP Employee

Look at attached files.

Use "Help" "Install New Software..." in Clipboard02.jpg file.

See available software using Clipboard04.jpg file.

 

It looks like you want to find QCVS.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,006 Views
kdo
Contributor I

Thank you very much for your answer,

I"d like to know some questions:

- Where is it possible to find the latest version the document QCVS

Processor Expert User Guide ???

The latest version dated 2016.

- Where is it possible to find the latest list of supported Freescale QorIQ

processors ?

With best regards.

Dmitry Konkov

SCANGROUP

+79859914365;

[email protected];

www.scangroup.ru;

0 Kudos
Reply

4,006 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Dmitry,

Processor expert is integrated in some of CW versions, thus user don't need install it separately.

What chip do you work with?

Which version of CodeWarrior do you work with?


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,006 Views
kdo
Contributor I

Hi,

thank you very much for your answer,

there are types Freescale (NXP) QorIQ processors:

p1022

p3041

p4080

p5040

The latest version of Code Warrior is 10.5.1. and Processor expert 4/5/x

With best regards

Dmitry Konkov

+79859914365;

[email protected];

www.scangroup.ru;

0 Kudos
Reply