default rom problem s12p

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

default rom problem s12p

1,444 Views
sprince
Contributor I

I am using the demos12pfame board from Freescale. Just for demonstrations purposes, I generate a new codwwarrior project, use device initialization, don't modify anything, then compile and launch the debugger.  If I change the debug config load to "verify memory image after loading code" I get error "loading verify failed at address 0x0008800."  Looking at the .prm file, the DEFAULT_ROM is placed into page 8.

 

But if I place the DEFAULT_ROM into ROM_C000 I don't get this error.  In my actual application, I need to have DEFAULT_ROM located in page 8 because my copy down is very large.

 

Why would this happen?

Labels (1)
0 Kudos
Reply
1 Reply

1,346 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Steward,

can you please upload your demo project for your problem? thanks!

Best Regards.

Jennie

0 Kudos
Reply