cyrillic with Codewarrior 6.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cyrillic with Codewarrior 6.3

ソリューションへジャンプ
2,332件の閲覧回数
cperez
Contributor I

I need to use Cyrillic words with WPC151 source, but I can't put this source in Codewarrior.

 

For Example. I need to compile this word.

НАСТРОЙКА

 

 

How I can use it??

 

 

Thanks in advance

ラベル(1)
1 解決策
2,244件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Carlos,

CW6.x does not support language packs.
CW10 itself doesn't support Russian either. but user can go to ( http://www.eclipse.org/ )

to find the additional language packs in Eclipse. only the strings localized (by the community) to Russian is supported.

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,245件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Carlos,

CW6.x does not support language packs.
CW10 itself doesn't support Russian either. but user can go to ( http://www.eclipse.org/ )

to find the additional language packs in Eclipse. only the strings localized (by the community) to Russian is supported.

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,244件の閲覧回数
cperez
Contributor I

Thanks for your response.

I'ts clear.

0 件の賞賛
返信
2,244件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Jennie Zhang

0 件の賞賛
返信