cwide.exe has stopped working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cwide.exe has stopped working

2,320 Views
740576674
Contributor I

Hi

I have the CW version 10.7 on Windows 10,and when i 'Edit' the connection in 'Flash File to Target',it appears a message "cwide.exe has  stopped working"and then  it  exit.and next time,there is no message, exist .

Also when I debug,it appears "the selection cannot be launched,and there is no recent launches"

I  tried reinstalling, but it did not work.

0 Kudos
Reply
3 Replies

2,158 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,158 Views
740576674
Contributor I

MC9S12ZVML128,

Thanks.

0 Kudos
Reply

2,158 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 孜文 张,

It seems the same case with your another thread CodeWarrior unable to launch 

I have reply you on that case.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply