connect P1010 with code warrior10.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

connect P1010 with code warrior10.5

2,315 次查看
silecy2016
Contributor I

Using Code Warrior 10.5 to connect the P1010, but failed.

Error : ELF is not in expected HALT mode

I use "P1010RDB_init_sram.tcl" to Initize P1010.

I need help, thanks.

1111.bmp

following is "P1010RDB_init_sram.tcl"

#########################################################################
# Initialization file for P1010RDB board - SRAM
# Clock Configuration:
# CPU: 1000 MHz, CCB: 400 MHz,
# DDR: 800 MHz, SYSCLK: 100 MHz
#########################################################################

variable CCSRBAR 0xff700000

proc CCSR {reg_off} {
global CCSRBAR

return p:0x[format %x [expr {$CCSRBAR + $reg_off}]]
}

proc apply_e500v2_workaround {} {
# After reset, e500 cores need to run before being able to enter debug mode.
# Work-around: set a HW BP at reset address and run the core; after the core hits the BP, it enters debug mode
# e500 cores need to have valid opcode at the interrupt vector

variable SPR_GROUP "e500 Special Purpose Registers/"
variable GPR_GROUP "General Purpose Registers/"
#######################################################################
# Set a breakpoint at the reset address
reg ${SPR_GROUP}IAC1 = 0xfffffffc
reg ${SPR_GROUP}DBCR0 = 0x40800000
reg ${SPR_GROUP}DBCR1 = 0x00000000

# Run the core
config runcontrolsync off
protocol ccs::run_core 0
wait 500
protocol ccs::stop_core 0
config runcontrolsync on
stop

# Clear affected registers
reg ${SPR_GROUP}DBSR = 0x01CF0000
reg ${SPR_GROUP}DBCR0 = 0x41000000
reg ${SPR_GROUP}IAC1 = 0x00000000
reg ${SPR_GROUP}CSRR0 = 0x00000000
reg ${SPR_GROUP}CSRR1 = 0x00000000
# Set the PC back to the reset address (for debug-->connect)
reg ${GPR_GROUP}PC = 0xfffffffc
}

proc init_board {} {

global CCSRBAR

# get ROM_LOC from PORBMSR
variable ROM_LOC 0x[format %x [expr {([mem [CCSR 0xE0004] -np] & 0x0f000000) >> 24}]]

##################################################################################
# configure internal SRAM at 0x00000000

# L2CTL
# bit 0 = 0 - L2E: L2 SRAM disabled
# bit 1 = 1 - L2I: L2 flash invalidate
# bit 2-3 = 01 - L2SIZ: = 256K
# bit 13-15 = 001 - L2SRAM: Entire array as SRAM (256K)
mem [CCSR 0x20000] = 0x50010000


# L2SRBAR0
# bit 0-17 = BASE addr: 0x00000000
mem [CCSR 0x20100] = 0x00000000

# L2SRBAREA0
# bit 28-31 = EXTENTED BASE addr: 0x00000000
mem [CCSR 0x20104] = 0x00000000

# L2CTL
# bit 0 = 1 - L2E: L2 SRAM enable
mem [CCSR 0x20000] = 0x90010000

##################################################################################
#
# Memory Windows
#
# 0xFE000000 0xFFFFFFFF LAW0 Local Bus NOR FLASH - 32M
# 0xEFB00000 0xEFBFFFFF LAW1 CPLD - 128K
# 0xEFA00000 0xEFAFFFFF LAW2 NAND - 16k
#
##################################################################################
# configure local access windows

# LAWBAR0 - IFC
# bit 8 - 31 = 0xFE000000 - base addr
mem [CCSR 0xC08] = 0x000fe000

# LAWAR0
# bit 0 = 1 - enable window
# bit 7-11 = 00100 - Local Bus
# bit 26 - 31 = 011000 32M - size
mem [CCSR 0xC10] = 0x80400018

# LAWBAR1 - CPLD
# bit 8 - 31 = 0xEFB00000 - base addr
mem [CCSR 0xC28] = 0x000efb00

# LAWAR1
# bit 0 = 1 - enable window
# bit 7-11 = 00100 - Local Bus
# bit 26-31 = 010000 128k - size
mem [CCSR 0xC30] = 0x80400010

# LAWBAR2 - Local Bus
# bit 8 - 31 = 0xEFA00000 - base addr
mem [CCSR 0xC48] = 0x00efa00

# LAWAR2
# bit 0 = 1 - enable window
# bit 7-11 = 00100 - IFC
# bit 26-31 = 010011 1M - size
mem [CCSR 0xC50] = 0x80400013

#######################################
# CPLD INIT
#######################################

config MemAccess 8
config MemWidth 8
mem v:0xefb00009 = 0x00
mem v:0xefb00013 = 0x00
config MemAccess 32
config MemWidth 32

##################################################################################
# added workaround for Errata ID - GEN-A016 (A-003549)
# PMUXCR
mem [CCSR 0xE0060] = 0x000000c0

##################################################################################
# configure IFC controller

# Autodetect CS routing based on ROM_LOC
# bits 4-7 - ROM_LOC
# 1000 8-bit NAND—512b page size
# 1001 8-bit NAND—2K page size
# 1010 8-bit NAND—4K page size
# 1011 8-bit NOR
# 1100 16-bit NAND—512b page size
# 1101 16-bit NAND—2K page size
# 1110 16-bit NAND—4K page size
# 1111 16b NOR

# boot location is NAND => NAND - cS0, NOR - CS1
if {($ROM_LOC >= 0x8 && $ROM_LOC <= 0xA) || (($ROM_LOC >= 0xC && $ROM_LOC <= 0xE))} {

###########################
# CS0 - NAND Flash settings

# AMASK0 64k NAND Flash buffer size
mem [CCSR 0x1E0A0] = 0xFFFF0000

# CSOR0
mem [CCSR 0x1E130] = 0x0110A200

#FTIM0_CS0
mem [CCSR 0x1E1C0] = 0x0E18070A
#FTIM1_CS0
mem [CCSR 0x1E1C4] = 0x32390E18
#FTIM2_CS0
mem [CCSR 0x1E1C8] = 0x01E0501E
#FTIM3_CS0
mem [CCSR 0x1E1CC] = 0x00000000

# CSPR0
mem [CCSR 0x1E010] = 0xEFA00083

##########################
# CS1 - NOR Flash settings

# AMASK1 32M NOR
mem [CCSR 0x1E0AC] = 0xFE000000

# CSOR1
mem [CCSR 0x1E13C] = 0x0000E000

#FTIM0_CS1
mem [CCSR 0x1E1F0] = 0x40050005
#FTIM1_CS1
mem [CCSR 0x1E1F4] = 0x1E000F00
#FTIM2_CS1
mem [CCSR 0x1E1F8] = 0x0410001C
#FTIM3_CS1
mem [CCSR 0x1E1FC] = 0x00000000

# CSPR1
mem [CCSR 0x1E01C] = 0xFE000105

} else {

##########################
# CS0 - NOR Flash settings

# AMASK0 32M NOR
mem [CCSR 0x1E0A0] = 0xFE000000

# CSOR0
mem [CCSR 0x1E130] = 0x0000E000

#FTIM0_CS0
mem [CCSR 0x1E1C0] = 0x40050005
#FTIM1_CS0
mem [CCSR 0x1E1C4] = 0x1E000F00
#FTIM2_CS0
mem [CCSR 0x1E1C8] = 0x0410001C
#FTIM3_CS0
mem [CCSR 0x1E1CC] = 0x00000000


# CSPR0
mem [CCSR 0x1E010] = 0xFE000105

###########################
# CS1 - NAND Flash settings

# AMASK1 64k NAND Flash buffer size
mem [CCSR 0x1E0AC] = 0xFFFF0000

# CSOR1
mem [CCSR 0x1E13C] = 0x0110A200

#FTIM0_CS1
mem [CCSR 0x1E1F0] = 0x0E18070A
#FTIM1_CS1
mem [CCSR 0x1E1F4] = 0x32390E18
#FTIM2_CS1
mem [CCSR 0x1E1F8] = 0x01E0501E
#FTIM3_CS1
mem [CCSR 0x1E1FC] = 0x00000000

# CSPR1
mem [CCSR 0x1E01C] = 0xEFA00083
}

# CS3 - CPLD
#CSPR3 base address at 0xEFB00000, valid
mem [CCSR 0x1E034] = 0xEFB00085
#AMASK3 64K
mem [CCSR 0x1E0C4] = 0xFFFF0000
#CSOR3
mem [CCSR 0x1E154] = 0x00000000

#FTIM0_CS3
mem [CCSR 0x1E250] = 0xe00e000e
#FTIM1_CS3
mem [CCSR 0x1E254] = 0x0e001f00
#FTIM2_CS3
mem [CCSR 0x1E258] = 0x0e00001f
#FTIM3_CS3
mem [CCSR 0x1E25C] = 0x00000000

#GCR
mem [CCSR 0x1E40C] = 0x00002800
#CCR
mem [CCSR 0x1E44C] = 0x03008000


#SPI init
# SPMODE
mem [CCSR 0x7000] = 0x80000403
# SPIM - catch all events
mem [CCSR 0x7008] = 0x00000000
# SPMODE1
mem [CCSR 0x7020] = 0x28170008
}

proc P1010RDB_init_core {} {
global CCSRBAR

variable SPR_GROUP "e500 Special Purpose Registers/"
variable SSP_GROUP "Standard Special Purpose Registers/"
variable CAM_GROUP "regPPCTLB1/"
variable GPR_GROUP "General Purpose Registers/"

##################################################################################
# move CCSR at 0xE0000000

# CCSRBAR
# bit 8 - 23 - BASE_ADDR
mem [CCSR 0x0] = 0x000e0000
set CCSRBAR 0xe0000000

######################################################################
# invalidate BR0
# CSPR0
mem [CCSR 0x1E010] = 0x00000100

# ABIST off
# L2ERRDIS[MBECCDIS]=1 L2ERRDIS[SBECCDIS]=1
mem [CCSR 0x20E44] = 0x0000000C

# activate debug interrupt and enable SPU
reg ${SSP_GROUP}MSR = 0x02000200

##################################################################################
#
# Memory Map
#
# 0x00000000 0x0003FFFF SRAM 256K
# 0xE0000000 0xE00FFFFF CCSRBAR Space 1M
# 0xEFA00000 0xEFA03FFF NAND 16k
# 0xEFB00000 0xEFBFFFFF Board CPLD 1M
# 0xFE000000 0xFFFFFFFF LocalBus NOR FLASH 32M
#
##################################################################################
# MMU initialization

# define 16MB TLB entry 0: 0xFF000000 - 0xFFFFFFFF; for Local Bus, cache inhibited, guarded
reg ${CAM_GROUP}L2MMU_CAM0 = 0x70000FCAFC080000FF000000FF000001

# define 16MB TLB entry 1: 0xFE000000 - 0xFEFFFFFF; for Local Bus, cache inhibited, guarded
reg ${CAM_GROUP}L2MMU_CAM1 = 0x70000FCAFC080000FE000000FE000001

# define 1MB TLB entry 2: 0xE0000000 - 0xE00FFFFF; for CCSR Space, non cacheable
reg ${CAM_GROUP}L2MMU_CAM2 = 0x500003CAFC080000E0000000E0000001

# define 256KB TLB entry 3: 0x00000000 - 0x0003FFFF; for internal chip SRAM
reg ${CAM_GROUP}L2MMU_CAM3 = 0x400001C0FC0800000000000000000001

# define 256KB TLB1 entry 4: 0xEFB00000 - 0xEFB3FFFF; for CPLD, cache inhibited, guarded
reg ${CAM_GROUP}L2MMU_CAM4 = 0x400001CA1C080000EFB00000EFB00001

# define 1MB TLB1 entry 5: 0xEFA00000 - 0xEFAFFFF; for NAND cache inhibited, guarded
reg ${CAM_GROUP}L2MMU_CAM5 = 0x500003CA1C080000EFA00000EFA00001

##################################################################################
# disable Boot Page Translation Register
mem [CCSR 0x20] = 0x00000000

# Invalidate again CSPR0 to prevent flash data damage in case
# the boot sequencer re-enables CS0 access
mem [CCSR 0x1E010] = 0x00000100

init_board

####################################################################
# interrupt vectors initialization
# IVPR (default reset value)
reg ${SPR_GROUP}IVPR = 0x00000000

# interrupt vector offset registers
# IVOR0 - critical input
reg ${SPR_GROUP}IVOR0 = 0x00000100
# IVOR1 - machine check
reg ${SPR_GROUP}IVOR1 = 0x00000200
# IVOR2 - data storage
reg ${SPR_GROUP}IVOR2 = 0x00000300
# IVOR3 - instruction storage
reg ${SPR_GROUP}IVOR3 = 0x00000400
# IVOR4 - external input
reg ${SPR_GROUP}IVOR4 = 0x00000500
# IVOR5 - alignment
reg ${SPR_GROUP}IVOR5 = 0x00000600
# IVOR6 - program
reg ${SPR_GROUP}IVOR6 = 0x00000700
# IVOR8 - system call
reg ${SPR_GROUP}IVOR8 = 0x00000c00
# IVOR10 - decrementer
reg ${SPR_GROUP}IVOR10 = 0x00000900
# IVOR11 - fixed-interval timer interrupt
reg ${SPR_GROUP}IVOR11 = 0x00000f00
# IVOR12 - watchdog timer interrupt
reg ${SPR_GROUP}IVOR12 = 0x00000b00
# IVOR13 - data TLB errror
reg ${SPR_GROUP}IVOR13 = 0x00001100
# IVOR14 - instruction TLB error
reg ${SPR_GROUP}IVOR14 = 0x00001000
# IVOR15 - debug
reg ${SPR_GROUP}IVOR15 = 0x00001500
# IVOR32 - SPE-APU unavailable
reg ${SPR_GROUP}IVOR32 = 0x00001600
# IVOR33 - SPE-floating point data exception
reg ${SPR_GROUP}IVOR33 = 0x00001700
# IVOR34 - SPE-floating point round exception
reg ${SPR_GROUP}IVOR34 = 0x00001800
# IVOR35 - performance monitor
reg ${SPR_GROUP}IVOR35 = 0x00001900

# put a valid opcode at debug and program exception vector address
mem v:0x00000700 = 0x48000000
mem v:0x00001500 = 0x48000000

##################################################################################
apply_e500v2_workaround

#############
#
# activate debug interrupt and enable SPU
reg ${SSP_GROUP}MSR = 0x02001200

############
#
# time base enable & MAS7 update
# HID0
reg ${SPR_GROUP}HID0 = 0x00004080

######
# CW debugger settings
#
#Trap debug event enable
reg ${SPR_GROUP}DBCR0 = 0x41000000

# for debugging starting at program entry point when stack is not initialized
reg ${GPR_GROUP}SP = 0x0000000F
}

proc envsetup {} {
# Environment Setup
radix x
config hexprefix 0x
config MemIdentifier v
config MemWidth 32
config MemAccess 32
config MemSwap off
}

#-------------------------------------------------------------------------------
# Main
#-------------------------------------------------------------------------------

envsetup

P1010RDB_init_core

0 项奖励
回复
1 回复

2,098 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Probably there is JTAG hardware design problem on your target board, please refer to page 6 in the attached ppt to check the hardware design, especially HRESET and TRST signals.

If your problem remains, please refer to the following procedure to capture your CCS log to me to do more investigation.

Please enable CCS log from "Run->Debug Configurations -><project>-core0_RAM_-Connect(Download)->Edit...->Advanced->Advanced CCS setting->Enable logging", and connect to the target from "Run->Debug Configurations-><project>-core0_RAM_-Connect(Download)->Debug”, the CCS log will be displayed in the console panel in CodeWarrior IDE. If you didn't find anything in the console, please open the panel from Window->Show View->Console, if the CCS log in the console is truncated, please enlarge the console buffer from Window->Preferences->Run/Debug->Console->uncheck "Limit console output".

Thanks,

Yiping

0 项奖励
回复