configuration download speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

configuration download speed

2,291 Views
haroldvogel
Contributor II

Sometimes I will receive a dialog box when the system fails to load code to the board I am working on.  The dialog box allows for a 'Reset', 'Abort', 'Retry', and other selections.  How can I bring up this dialog box so that I can change the download speed.

Labels (1)
0 Kudos
Reply
3 Replies

2,184 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please check if attached video includes what you are looking for?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,184 Views
haroldvogel
Contributor II

Yes, that helps.

John Vogel

0 Kudos
Reply

2,184 Views
haroldvogel
Contributor II

Here is a snap shot of the dialog box:

pastedImage_0.png

This is the dialog box I am trying to open.

0 Kudos
Reply