configuration and data reading from TWR-LCD touch screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

configuration and data reading from TWR-LCD touch screen

1,435件の閲覧回数
ankurchauhan
Contributor I

Hi,

I'm using K70 TWR development kit and twr-lcd(resistive touch) module.

I'm using bate metal project with CW 10.6.4.

I have a sample project of CW 6.3

 

where they are using following function :

D4D_Init();

D4D_SetOrientation();

D4D_CalibrateTouchScreen();

D4D_Poll();

 

to read the data from screen.

 

Can i also use these function in my project.

 

 

Regards

Ankur

ラベル(1)
0 件の賞賛
返信
1 返信

1,359件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Ankur,

For the eGUI I recommend you to refer to the link

    Gargy007/eGUI · GitHub

This is better community for eGUI.

Also you will find some info under the web site:

    www.nxp.com/egui


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信