USB Multilink versis Tower.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Multilink versis Tower.

1,400 Views
dennisdice
Contributor I

@

I am use to using the USB Multilink from P& E.  That is all over now, I have to use the Tower system and make my PC board as big as the tower foot print. If I want to develop with ur micros.

Dennis Dice

Labels (1)
0 Kudos
Reply
1 Reply

1,284 Views
trytohelp
NXP Employee
NXP Employee

Hi Dennis,

Most of the time the TWR board includes the OSBDM port and BDM/Jtag post.

By this way you can use the OSBDM (sample UBS cable between the PC and board) or a P&E interface as Multilink Universal.

If you are using CodeWarrior or KDS, the project wizard propose you to select both interfaces.

You will find more details under P&E web site:

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Hope this will help


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply