codewarrior usb tap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

codewarrior usb tap

2,288件の閲覧回数
zbxggs
Contributor II

hello,

Over the years, we have been using CodeWarrior v8.8 and codewarrior usb tap to program the external flash of mpc8323. However, with the aging and damage of the codewarrior usb tap, we have only one usb tap can work now, so we want to confirm the following problems:

① Is the CodeWarrior USB tap we used in the picture attached stopped production? If the production has been stopped, is there still any way to buy it?

② If we use cwh-ctp-base-he + cwh-ctp-cop-ye to replace CodeWarrior USB tap, do we need to install other drivers or patch files for the original settings or CodeWarrior 8.8 software??微信图片_20200701125004.jpg 

0 件の賞賛
返信
1 返信

2,221件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is the CodeWarrior USB tap we used in the picture attached stopped production?

Yes.

> If the production has been stopped, is there still any way to buy it?

NXP does not sell obsolete products - try to search third-party vendors.

> If we use cwh-ctp-base-he + cwh-ctp-cop-ye to replace CodeWarrior USB tap,

> do we need to install other drivers or

> patch files for the original settings or CodeWarrior 8.8 software??

No.

0 件の賞賛
返信