codewarrior 5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior 5.1

13,646 Views
rajkumarvinodka
Contributor II

I am trying to install Codewarrior 5.1 on my Windows-7 64-bit machine.

The package from the web shows the following files to be installed as a part of 5.1

 

148656_148656.pngpastedImage_0.png

 

When I begin installation, the following files were installed in sequence:-

  • CodeWarrior for HCS12(X) Microcontrollers v5.1.exe
  • CodeWarrior for HCS12 v5.1 Compiler Update.exe
  • CodeWarrior for HCS12 v5.1 G240 Service Pack.exe
  • CodeWarrior for HCS12 v5.1 VR64 Service Pack.exe
  • CodeWarrior for HCS12 v5.1 GA128GN32 Service Pack.exe

 

The next one that I tried was:-

  • CodeWarrior for HCS12 v5.1 G64 Service Pack.exe

executing which resulted in the below alert window popping, that I decided to skip (clicked the "No" button) this one. I don't know where to find this "Processor Expert v3.03 Service Pack"

148657_148657.pngpastedImage_3.png

The next one I tried was Processor Expert updates V3.05 for CodeWarrior for HCS12 v5.1.exe, and the installation got stuck at the below now. Looks like this needs the previous step to be successful in order for this one to succeed.

148685_148685.pngpastedImage_7.png

 

What should be the exact installation sequence? And what other files (than listed in the website on 5.1) would be required and where to find them?

One more, is the Codewarrior 5.1 designed to function well with Windows-7 (ot 8 or 10) 64-bit?

Labels (1)
10 Replies

9,817 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The CW12_V5_1_PE_V3_03_SP.exe is too large , so it can not attached on the community,

please share me a email , i can send to you .

Hope it hleps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,817 Views
rajkumarvinodka
Contributor II

Alice,

And, would also like to know the CodeWarrior 5.1 ‘s support for the following operating systems: Windows7, Windows8 and Windows10.

Thanks

Vinod

0 Kudos
Reply

9,817 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vinod,

Please download it at here : http://pan.baidu.com/s/1hsIw2aC

after click thin linker ,please click here :

pastedImage_1.png

And the cw5.1 does not support the Windows8 and Windows10, you can check the release note :

Freescale\CWS12v5.1\HCS12X_Quick_Start.pdf

pastedImage_2.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

9,817 Views
rajkumarvinodka
Contributor II

Hi Alice,

Along with sending me the CW12_V5_1_PE_V3_03_SP.zip file,

Kindle do please let us know what flash programmers/debuggers are compatible with Codewarrior 5.1 that we could use with the chip MC9S12DG128CPVE.

Thanks

Vinod

0 Kudos
Reply

9,810 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Rajkumar,

I have send to you by my personal email , please check .

Hope it helps

Alice

0 Kudos
Reply

9,810 Views
rajkumarvinodka
Contributor II

Thanks, but this is sad.

If I will need to be buying one license, and a portion of the software comes from a non-NXP website - how should I be expecting support/ownership for such a product from NXP now?

I have started the download anyways, will let you know how it behaves.

0 Kudos
Reply

9,810 Views
rajkumarvinodka
Contributor II

Hello Alice,

I can’t understand the website.

Please send it to vinod.kanna@alpha.ca

Also please send me the release notes of 5.1

Did you just mention Codewarrior 5.1 does not support Windows 8 and Windows 10?

Thanks

Rajkumar Vinod Kanna

Mobile: +91-9980523712

0 Kudos
Reply

9,810 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The CW12_V5_1_PE_V3_03_SP.exe is too large , it can not send by email also .

You do not need understand the web , you only need click it refer to the screenshot :

pastedImage_0.png

pastedImage_1.png

- About the DOC,  under the CW installation directory you can find , i also attach it for you.

- About the debugger , you can use these :

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

BR

Alice

0 Kudos
Reply

9,810 Views
rajkumarvinodka
Contributor II

Hi Alice,

I tried to do that, I get one more pop window from the website as shown below.

I don’t understand this. Where is this in the NXP website that I could downloaded?

Thanks

Rajkumar Vinod Kanna

Mobile: +91-9980523712

0 Kudos
Reply

9,810 Views
rajkumarvinodka
Contributor II

Hello Alice,

I could not find the attachment.

Could you please send it to vinod.kanna@alpha.ca<mailto:vinod.kanna@alpha.ca> ?

Thanks

Vinod

0 Kudos
Reply