codewarrior 10.6 with codewarrior 10.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

codewarrior 10.6 with codewarrior 10.4

ソリューションへジャンプ
2,005件の閲覧回数
mlockner
Contributor I

Can I have both codewarrior 10.6 and codewarrior 10.4 installed on the same computer? I have an old project that was done with 10.4 and I have the need to help on a project that was started with 10.6.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,711件の閲覧回数
BlackNight
NXP Employee
NXP Employee

yes. I'm using that all the time.

I recommend that for each IDE/CW you have its own workspace, e.g.

- wsp_10.6

- wsp_10.4

so you keep the IDE settings/etc separate. Mixing workspaces with different Eclipse versions is a bad thing.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,712件の閲覧回数
BlackNight
NXP Employee
NXP Employee

yes. I'm using that all the time.

I recommend that for each IDE/CW you have its own workspace, e.g.

- wsp_10.6

- wsp_10.4

so you keep the IDE settings/etc separate. Mixing workspaces with different Eclipse versions is a bad thing.

Erich

0 件の賞賛
返信