codewarrior 10.6 with codewarrior 10.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior 10.6 with codewarrior 10.4

Jump to solution
1,987 Views
mlockner
Contributor I

Can I have both codewarrior 10.6 and codewarrior 10.4 installed on the same computer? I have an old project that was done with 10.4 and I have the need to help on a project that was started with 10.6.

Labels (1)
0 Kudos
Reply
1 Solution
1,693 Views
BlackNight
NXP Employee
NXP Employee

yes. I'm using that all the time.

I recommend that for each IDE/CW you have its own workspace, e.g.

- wsp_10.6

- wsp_10.4

so you keep the IDE settings/etc separate. Mixing workspaces with different Eclipse versions is a bad thing.

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,694 Views
BlackNight
NXP Employee
NXP Employee

yes. I'm using that all the time.

I recommend that for each IDE/CW you have its own workspace, e.g.

- wsp_10.6

- wsp_10.4

so you keep the IDE settings/etc separate. Mixing workspaces with different Eclipse versions is a bad thing.

Erich

0 Kudos
Reply