code warrior instalation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

code warrior instalation

2,120 次查看
tonymoseby
Contributor II

Hello, I am trying to install code warrior in a i386 machine wit ubuntu 14:04 32 bits.

I get this fault:

I have checked that my java is a 32 bits  java...what could the problem be!

Thansk for your helo

sudo ./setuplinux.sh Unpacking JRE ... Starting Installer ... /home/roca/Downloads/codewarrior/disk1/setuplinux.sh.6078.dir/jre/bin/java: 1: /home/roca/Downloads/codewarrior/disk1/setuplinux.sh.6078.dir/jre/bin/java: Syntax error: end of file unexpected (expecting ")")

标签 (1)
3 回复数

1,970 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tony,

Could you tell us which MCU are you using?

Please notice that the latest CodeWarrior version with Linux support was CodeWarrior 10.2 and it was only tested on Red Hat Enterprise Edition 5.4 (32-bit and 64-bit) and Ubuntu 10.04 (32-bit and 64-bit). If you are using a Kinetis device it may be a better option to use Kinetis Design Studio, which comes with support for Red Hat® Enterprise Linux (RHEL), CentOS 6.4 and Ubuntu 14.04 LTS. These linux-hosted variants of the Kinetis Design Studio software development
tools are distributed as 64-bit binaries, which will not work on 32-bit systems.

Kinetis Design Studio Integrated Development Environment (IDE)|NXP 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

1,970 次查看
tonymoseby
Contributor II

Hi,Thanks for a good answer,  I want to compile an application(protocol stack) for a LS1021A development kit, I can see that codewarrior supports(compiles) this device.Question is does Kinetics design studio supports it?ThanksBr/T

Den fredag, 14 oktober 2016 1:42 skrev Carlos_Mendoza <[email protected]>:

#yiv4677073350 * #yiv4677073350 a #yiv4677073350 body {font-family:Helvetica, Arial, sans-serif;}#yiv4677073350 #yiv4677073350 h1, #yiv4677073350 h2, #yiv4677073350 h3, #yiv4677073350 h4, #yiv4677073350 h5, #yiv4677073350 h6, #yiv4677073350 p, #yiv4677073350 hr {}#yiv4677073350 .yiv4677073350button td {}

|

NXP Community

|

Re: code warrior instalation

reply from Carlos_Mendoza in CodeWarrior Development Tools - View the full discussionHi Tony, Could you tell us which MCU are you using? Please notice that the latest CodeWarrior version with Linux support was CodeWarrior 10.2 and it was only tested on Red Hat Enterprise Edition 5.4 (32-bit and 64-bit) and Ubuntu 10.04 (32-bit and 64-bit). If you are using a Kinetis device it may be a better option to use Kinetis Design Studio, which comes with support for Red Hat® Enterprise Linux (RHEL), CentOS 6.4 and Ubuntu 14.04 LTS. These linux-hosted variants of the Kinetis Design Studio software development

tools are distributed as 64-bit binaries, which will not work on 32-bit systems. Kinetis Design Studio Integrated Development Environment (IDE)|NXP 

Hope it helps! Best Regards,

Carlos Mendoza

Technical Support Engineer

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in CodeWarrior Development Tools by email or at NXP Community

Following Re: code warrior instalation in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences |

|

0 项奖励
回复

1,970 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tony,

Thanks for your response. Unfortunately KDS does not support the LS1021A processors but it is supported by CodeWarrior Development Studio for QorIQ LS series for ARM v7 ISA v10.0.8. You should be able to install this CodeWarrior version on Ubuntu, the supported operating systems are:

- Windows® 7 SP1 or later systems. Includes 32-bit and 64-bit
- Ubuntu 64-bit OS: Supports the latest LTS version or within four months of LTS release.
- Redhat 64-bit: Latest LTS version or within four months of LTS release.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复