code warrior for Ubuntu 14 ???..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code warrior for Ubuntu 14 ???..

2,585件の閲覧回数
rogercovarrubia
Contributor III

Is there a code warrior 2.10  version for ubuntu 14? I use the MPC5606B and I use code warrior 2.10  on windows but I was wondering if there is a version for ubuntu??

 

 

thanks!!

 


Roger

ラベル(1)
2 返答(返信)

2,323件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

CodeWarrior v2.10 does not support Ubuntu, it only works for Windows  XP/Vista/7.  We have Eclipse CodeWarrior v10.2 which supports Ubuntu v10.04. But CodeWarrior v10.2 only supports parts of Qorivva device, including MPC560xP, MPC56xxF, MPC567xK, MPC5643L, MPC56xxS, MPC5668E/G. But it does not support  MPC560xB. Sorry for this inconvenience.

2,323件の閲覧回数
rogercovarrubia
Contributor III

thanks

0 件の賞賛
返信