change MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

change MCU

2,298件の閲覧回数
wba
Contributor III


In CW6 there was a button to change MCU.  How do I change MCU in CW10?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,191件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Bruce:

In CW v10.x (Eclipse), there is not a direct method to change the target CPU of a project.

The recommended procedure is always to create a new project for the desired device and copy the source and header files from the original project.

If using Processor Expert, then there is an alternative to do this; check the next tutorial by colleague Erich Styger:

Changing the CPU with Processor Expert | MCU on Eclipse


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,191件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Could you please attach a screenshot to show this button? Thanks!

0 件の賞賛
返信