ccs protocol plugin::could not connect to the requested core core#0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ccs protocol plugin::could not connect to the requested core core#0

3,893 Views
maheshwarreddy
Contributor I

We are using the MPC 860 power pc QUICC processor we are using the code warrior IDE for debugging . While entering into the debug we are getting an error as below .Find the below attachment for the CCS log.

Thank you 

Best regards 

Maheshwar

0 Kudos
Reply
1 Reply

3,671 Views
Pavel
NXP Employee
NXP Employee

Test CCS connection to your board using the following commands in CCS console:

 (bin) 49 % config cc cwtap

(bin) 50 % show cc

 

The following commands also can be used:

(bin) 49 % log v

(bin) 50 % source IDcode.tcl

 

Is there connection to the CodeWarrior TAP and MPC860 if these commands are used?

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply