cannot access projects on my cloud drive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot access projects on my cloud drive

2,127 Views
juliancox
Contributor V

How do I access projects that are stored on my cloud drive. CW does not see the cloud drive, but Windows does. It was fine with CW10.7, but not with CW 11. Now it does not work with either

0 Kudos
Reply
3 Replies

1,777 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox,

Which chip do you development ?

0 Kudos
Reply

1,777 Views
juliancox
Contributor V

I am using S08QE16.

I installed CW 10.7 on a new machine and it can see everything on my cloud drive (Dropbox). However :-

I imported my project into a new workspace (without the "copy files into the workspace" option. It imported OK and I can see, edit and compile my source files. When I do a build I get several errors;

"FATAL C50: Input file 'Sources/Events.args' not found"

There are similar errors for "main", "events" and two of the Processor Expert components, but all of the files are there in the project and I can see their content in the editor window.

Why doesn't CW like me???????

0 Kudos
Reply

1,777 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian,

Sorry I haven't use the Dropbox, while I'm glad to talking with you about this issure.

Please check the input path :

pastedImage_1.png

also check the "Build Variables":

pastedImage_1.png

And could you please take a screenshot to  tell me when import the project in cloud , how to choose it? I want to test on my side to check the issure.

BR

Alice

0 Kudos
Reply