can't declare a static matrix bigger than 49x16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can't declare a static matrix bigger than 49x16

ソリューションへジャンプ
1,608件の閲覧回数
juanignaciotroi
Contributor III

Hello. I am developing using the FRDM KE02 and I have the following problem. In my project, I have a printer in which I need the ascii characters from the 0x20 (space) to the 0x7A (z). This is a total of 91 characters. In orden to print them correctly, each character is a vector of 16 bytes. This is why I need a 91x16 matrix to describe all the characters I need.

 

However, when I want to declare this static matrix as:

 

unsigned int MATRIX_CHARACTERS[91][16 ] = {{},{},...,.{}}; as a global variable, it doesn't compile.

 

The error is: "c:/freescale/cw mcu v10.6/cross_tools/arm-none-eabi-gcc-4_7_3/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: region `m_data' overflowed by 2660 bytes"

 

How can I solve this problem?

 

I need this matrix to be static and to be in memory code.

 

Thank you, Juan Ignacio Troisi

ラベル(1)
0 件の賞賛
返信
1 解決策
1,533件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Juan,

the error means that you are using more RAM than you have available.

Why is your array an array of int? char should be enough? that would be 4 times less memory :-)

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,534件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Juan,

the error means that you are using more RAM than you have available.

Why is your array an array of int? char should be enough? that would be 4 times less memory :-)

Erich

0 件の賞賛
返信